DOCA0037EN-13

Menu Structure

Menu Types

FDM128 menus are divided into two types:

  • Settings menus: blue title bar background

  • Operation menus: green title bar background

Settings Menus

Settings menus are composed of two sequences:

  • General settings sequence

  • Settings sequence for devices: communication settings, device discovery, and editing devices

The setting wizard of the FDM128 display guides you through these sequences.

General View

The General view menu is used to monitor up to eight devices at the same time.

For further information, refer to the general view topic.

Device View

Device view menus are only accessible from the General view menu.

The Device view for circuit breakers menu is composed of the following submenus:

The Device view for Smartlink SI B menu is composed of the following submenus:

The Device view for Smartlink SI D menu is composed of PowerTag submenu.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?