General View
Overview
The menu allows you to monitor up to eight selected devices through summarized information.
There are two display modes:
-
Icon
-
List
Switch between display modes by pressing the corresponding icon in the lower right corner of the screen.
From this menu, you can reach the screens of the monitored devices:
-
Device view for ComPacT, PowerPacT , MasterPacT circuit breakers.
-
Device view for Smartlink devices.
Icon Mode
In the icon mode, the eight devices are displayed on one screen, each one by an icon.
To reach a , press the corresponding icon.
List Mode
In the list mode, four devices are displayed per screen, one per line.
Locating Intelligent Modular Units
@DTP: SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
The FDM128 display enables you to identify a circuit breaker that is part of a monitored intelligent modular unit (IMU), by making its MicroLogic trip unit or FDM121 display blink.
To locate an IMU:
Viewing Devices Updated Remotely
The FDM128 display can display the names of the circuit breakers and the name of the Smartlink SI B , Smartlink SI D , and Smartlink Modbus gateway that they are connected to. The names can be remotely updated using EcoStruxure Power Commission software. In this case, you have to refresh the displayed names to see the new names.
To refresh the display of names, press
. A progress bar is displayed
while the screen is refreshed.
In networks where names can be updated at anytime, it is recommended to refresh the FDM128 display periodically.
ERMS Status for MasterPacT MTZ Circuit Breaker
The ERMS status is displayed in the for a MasterPacT MTZ circuit breaker.
Icon Mode
In the icon mode, the device with its ERMS mode engaged displays a blue ERMS message below the device icon.
To reach a , press the corresponding icon.
List Mode
In the list mode, the device with its ERMS mode engaged displays the Ir settings in blue.
To reach , press
on the corresponding line.
Device View
In the , the device with its ERMS mode engaged displays an ERMS message in the title bar.




To Do: Pierre to confirm if it is necessary to complete Device view for switch-disconnectors.