DOCA0037EN-13

Overview

Presentation

The FDM128 Ethernet display for eight devices is a 1-to-8 human machine interface (HMI). The main component is a 5.7-inch touch screen.

for DTP team, on SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"

An FDM128 display can be connected to devices via an Ethernet interface by using:

  • One or more Ethernet gateways (IFE server, Link150, PowerLogic EGX300 and EGX100 Ethernet, PowerTag Link, EcoStruxure Panel Sever, Smartlink SI B , Smartlink SI D , or Smartlink Ethernet gateways).

  • One or more third-party Ethernet gateways that possess the appropriate characteristics.

NOTE: FDM128 display does not support devices with local ID (Virtual ID) from the Com'X or Link150 gateways.

Each type of connection is described further in this section.

for DTP team, on SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"

The FDM128 display can monitor and control up to eight devices. The information displayed includes measurements, alarms, and operating assistance data.

For ease of installation, a device discovery function is embedded in the FDM128 display .

Number and Nature of Connected Devices

Up to eight devices from the following list can be monitored simultaneously:

  • MasterPacT MTZ circuit breakers

  • MasterPacT NT/NW circuit breakers or switch-disconnectors

  • ComPacT NS 1600b-3200 circuit breakers or switch-disconnectors

  • ComPacT NS 630b-1600 circuit breakers or switch-disconnectors

  • PowerPacT P- and R-frame circuit breakers

  • ComPacT NSX circuit breakers or switch-disconnectors

  • PowerPacT H-, J-, and L-frame circuit breakers

  • Smartlink SI B gateway

  • Smartlink SI D gateway

  • Smartlink Modbus gateway

  • PowerTag Link gateway

  • PowerTag Link B gateway

  • PowerTag Link HD gateway

  • EcoStruxure Panel Server Universal

  • EcoStruxure Panel Server Advanced

  • EcoStruxure Panel Server Entry

NOTE: PowerTag Link B gateway is equivalent to Smartlink SI B gateway.

Monitored Devices Through Smartlink SI B Gateway

When an Smartlink SI B gateway is connected to the FDM128 display, the status of the devices connected through the gateway can be viewed on the FDM128 display.

The status of the following devices can be viewed on the FDM128 display:

  • Acti9 iOF+SD24 and OF+SD24 indication auxiliaries

  • Acti9 OF24 indication auxiliaries

  • Acti9 SD24 indication auxiliaries

  • Acti9 iACT24 and iATL24 auxiliaries for contactors and impulse relays in the Acti9 range

  • Acti9 RCA iC60 remote control module with Ti24 interface

  • Acti9 Reflex iC60 integrated control circuit breaker with Ti24 interface

  • PowerTag energy sensors, which are directly mounted on a Acti9 circuit breaker and communicate with the Smartlink SI B gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag energy sensors.

  • PowerTag M250/M630 energy sensors, which are directly mounted on a ComPacT NSX circuit breaker and communicate with the Smartlink SI B gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag M250/M630 energy sensors.

  • iEM2000T, iEM3110, iEM3155, iEM3210, and iEM3255 energy meters

  • ComPacT NSX OF+SD indication auxiliaries

NOTE: The Smartlink product range is not available in the following countries: United States, Canada, Mexico. Consult the catalog for the list of products available in your country.

Monitored Devices Through Smartlink SI D Gateway

When an Smartlink SI D gateway is connected to the FDM128 display, the status of the devices connected through the gateway can be viewed on the FDM128 display.

The status of the following devices can be viewed on the FDM128 display:

  • PowerTag 63 A energy sensors, which are directly mounted on a Acti9 circuit breaker and communicate with the Smartlink SI D gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag energy sensors.

  • PowerTag M250/M630 energy sensors, which are directly mounted on a ComPacT NSX circuit breaker and communicate with the Smartlink SI D gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag M250/M630 energy sensors.

NOTE: The Smartlink product range is not available in the following countries: United States, Canada, Mexico. Consult the catalog for the list of products available in your country.

Monitored Devices Through PowerTag Link Gateway

When a PowerTag Link gateway is connected to FDM128 display, the status of the devices connected through the gateway can be viewed on the FDM128 display.

The status of the following devices can be viewed on the FDM128 display:

  • PowerTag 63 A energy sensors, which are directly mounted on a Acti9 circuit breaker and communicate with the PowerTag Link gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag energy sensors.

  • PowerTag M250/M630 energy sensors, which are directly mounted on a ComPacT NSX circuit breaker and communicate with the PowerTag Link gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag M250/M630 energy sensors.

  • PowerTag F160 energy sensor (A9MEM1580)

  • PowerTag Rope energy sensors (A9MEM1590, A9MEM1591, A9MEM1592, and A9MEM1593)

Monitored Devices Through EcoStruxure Panel Server Gateway

When an EcoStruxure Panel Server gateway is connected to FDM128 display, the status of the devices connected through the gateway can be viewed on the FDM128 display.

The status of the following devices can be viewed on the FDM128 display:

  • PowerTag 63 A energy sensors, which are directly mounted on a Acti9 circuit breaker and communicate with the EcoStruxure Panel Server gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag energy sensors.

  • PowerTag M250/M630 energy sensors, which are directly mounted on a ComPacT NSX circuit breaker and communicate with the EcoStruxure Panel Server gateway through wireless communication. Refer to the Component Part Numbers for the list of PowerTag M250/M630 energy sensors.

  • PowerTag F160 energy sensor (A9MEM1580)

  • PowerTag Rope energy sensors (A9MEM1590, A9MEM1591, A9MEM1592, and A9MEM1593)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?