Interface Specifications
USB1 Interface (USB Peripherals)
|
HOST Interface Characteristic |
Value |
|
|---|---|---|
|
Transmission speed |
High speed |
480 Mbps |
|
Full speed |
12 Mbps |
|
|
Low speed |
1.5 Mbps |
|
|
Maximum current supplied |
250 mA |
|
|
Maximum transmission distance |
5 m (16.40 ft) at 12 Mbps |
|
|
Connector |
USB Type-A V2.0 |
|
Ethernet Interface
|
LED |
Description |
|---|---|
|
Green 1 |
Link state |
|
Green 2 |
Activity |