DOCA0037EN-13

Browsing

Navigate Through the Screens

In a menu or a submenu, you can navigate through the screens by using the footer icons.

The browsing actions are executable by pressing the icons. Refer to the icon list to get the meaning of each of them.

The icons are available depending on the network configuration, the selected menu, and the possible actions.

NOTE: A gray icon means that the option or action is not available in the actual context.

Data Entry

When an action requires an alphanumeric entry (for example, typing a designation), the following touch keyboard is displayed:

When an action requires a numeric entry (for example, typing an IP address), the numeric keyboard is displayed.

NOTE: You can also display the numeric keyboard by pressing the 123 key on the alphanumeric keyboard.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?