Adding, Removing, and Replacing Devices
Adding New Devices
|
Step |
Action |
|---|---|
|
1 |
Ensure that settings of the new devices are compliant with the prerequisites. |
|
2 |
|
|
3 |
For devices connected through a gateway:
For devices connected directly: |
Removing Selected Devices
|
Step |
Action |
|---|---|
|
1 |
Disconnect the devices from the network. |
|
2 |
|
|
3 |
For devices connected through a gateway:
|
Replacing MicroLogic
|
Step |
Action |
|---|---|
|
1 |
Replace the MicroLogic trip unit. |
|
2 |
Press the |
|
3 |
For devices connected through a gateway:
|