Certifications and Standards
Introduction
Schneider Electric has submitted this product for independent testing and qualification by third-party listing agencies. These agencies have certified this product as meeting the following standards.
The FDM128 display is certified by the Underwriters Laboratories according to UL 508 for Industrial Control Equipment.
@DTP: SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
The FDM128 display is designed to comply with merchant navy bridge and deck requirements (refer to the Schneider Electric website for installation guidelines).
For detailed information, contact your local distributor or see the catalog and marking on the product.
Compliance with Standards
@DTP: SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
The FDM128 display complies with the following standards:
-
IEC 60947-1 general rules
-
UL 508, Industrial Control Equipment
-
CSA C22.2 No. 14-05 Industrial Control Equipment
-
IACS E10
Hazardous Substances
@DTP: SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
The FDM128 display is designed for compliance with the following directives and standards:
-
WEEE, Directive 2002/96/EC
-
RoHS, Directive 2002/95/EC
-
RoHS China, Standard SJ/T 11363-2006
UL Conditions of Acceptability for the FDM128 Display
@DTP: SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
The FDM128 display is suitable for use in hazardous locations in accordance with Class 1, Division 2 standards. All relevant local, state, and regional codes must be followed.
CE Markings
This product
conforms to the requirements for applying the
label.
WARNING |
|---|
|
RISK OF EXPLOSION IN HAZARDOUS LOCATIONS
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING
@DTP: SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"