Settings During Operation
General Settings
Setting functions that can be used during operation, without restarting the setting wizard, are:
-
Modifying the general settings
-
Editing devices
-
Adding single IP devices manually
Editing Devices
Limitations
When the following devices are used together, you cannot write or edit the device name:
-
MasterPacT NT/NW with BCM module, firmware version lower than 3.2.5.
-
ComPacT NS with BCM module, firmware version lower than 3.2.5.
-
PowerPacT P- and R-frame with BCM module, firmware version lower than 3.2.5.
An example network architecture is provided in this guide.
Prerequisites
Before editing devices, you must verify that the following prerequisites are met:
-
Circuit breaker must be in the remote control mode.
-
Device logging in the IFE or EIFE webpage must be disabled.
-
Only the following characters are allowed:
-
Upper case letters from A to Z
-
Lower case letters from a to z
-
Digits from 0 to 9
-
Hyphen -
-
-
Before editing the name and label of the circuit breaker:
-
The EIFE intrusive command mode must be unlocked
-
The locking pad of the IFE, or IFM interface must point to the open padlock, as shown in the following graphic
-
When the communication network is configured, access the menu by pressing
.
Use the menu to:
-
Provide a label for each device:
The label is defined in the field and is only displayed in the FDM128 display . The field contains up to 4 characters.
-
Rename a device:
The name is defined in field and is the actual name of the device. You may need to use the device password to rename the device. The field contains up to 12 characters.
Communications Settings
Use this menu to:
-
View the present communication settings configuration.
-
Restart the setting wizard, beginning at the point following the general settings, where you can modify the FDM128 display settings.
-
If the number of devices is less than eight, manually add an IFE interface, an EIFE interface, an Smartlink SI B gateway, or an Smartlink SI D gateway.
Access Code Settings
During operation, you can access the menu by pressing
. Use this menu to view and edit user login and access code
settings.