Device View for Devices Connected to the Smartlink Devices
Overview
For each submenu selected in the left tab of the main area, a headpiece allows you to navigate through the tabs. Press the corresponding tab title to display it.
Data displayed in the screen depends on the device connected to the Smartlink device. Refer to the relevant user guides provided in the section Related Documents.
Each Smartlink device concentrates data from connected devices on its channels.
The table lists the features available per device type:
|
Features |
Smartlink SI B |
Smartlink SI D PowerTag Link PowerTag Link HD |
Smartlink Modbus |
|---|---|---|---|
|
Control |
✓ |
– |
✓ |
|
Status |
✓ |
✓ |
✓ |
|
Counters |
✓ |
✓ |
✓ |
Monitoring Information
Depending on the type of the connected device, the displays:
-
The status of the connected device (only for Smartlink SI B and Smartlink Modbus devices)
-
The counters measured by the connected device (only for Smartlink SI B and Smartlink Modbus devices)
-
Buttons to control other devices connected to the Smartlink (only for Smartlink SI B and Smartlink Modbus devices)
-
Metering data provided by PowerTag energy sensors (only for Smartlink SI B , Smartlink SI D , and EcoStruxure Panel Server devices)
For example, the layout of the for a device connected to an Smartlink SI B gateway is as follows:
Control
DANGER |
|---|
|
RISK OF ELECTROCUTION, ELECTRIC ARC, OR BURNS
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
HAZARD OF CLOSING ON ELECTRICAL FAULT
Do not close the circuit breaker again without first inspecting
and, if necessary, repairing the downstream electrical equipment.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The procedure to control an Smartlink device is as follows:
|
Step |
Action |
|---|---|
|
1 |
In the submenu , press the action ( or ) for the target device. |
|
2 |
Press . The following operations occur:
|
|
3 |
Press to close the result popup. |
PowerTag 63 A for Acti9 Circuit Breakers
The FDM128 display scans, discovers, and shows data from up to:
-
20 PowerTag Energy sensors per Smartlink SI B , Smartlink SI D , or PowerTag Link (maximum gateway capacity is 20).
-
40 PowerTag Energy sensors per PowerTag Link HD or EcoStruxure Panel Server gateway (maximum gateway capacity is 100).
The FDM128 display can show data from a maximum of 8 gateways ( Smartlink SI B , Smartlink SI D , PowerTag Link, PowerTag Link HD, or EcoStruxure Panel Server gateway).
The data from each energy sensor is displayed on a dedicated page.
Depending on whether the PowerTag energy sensor is single-phase or three-phase, the following information is displayed in the submenu.
For single-phase PowerTag energy sensors:
-
Label
-
Asset name
-
Current (I)
-
Total active energy (Resettable)
-
Voltage status
-
Voltage (phase-to-neutral voltage)
For three-phase PowerTag energy sensors:
-
Label
-
Asset name
-
Current (I) among the phases Ia, Ib, and Ic
-
Total active energy (Resettable)
-
Voltage status
-
Average voltage (phase-to-phase voltage)
For three-phase and neutral PowerTag energy sensors:
-
Label
-
Asset name
-
Current (I) among the phases Ia, Ib, and Ic
-
Total active energy (Resettable)
-
Voltage status
-
Average voltage (phase-to-neutral voltage)
PowerTag for ComPacT NSX Circuit Breakers
The FDM128 display scans, discovers, and shows data from up to:
-
20 PowerTag M250/M630 energy sensors per Smartlink SI B , Smartlink SI D , or EcoStruxure Panel Server gateway.
-
40 PowerTag M250/M630 energy sensors per PowerTag Link HD gateway.
The data from each energy sensor is displayed on a dedicated page.
The following information is displayed in the submenu of PowerTag M250/M630 energy sensors:
-
Label
-
Asset name
-
Current (I)
-
Total active energy (Resettable)
-
Power Factor
-
Average voltage
-
Voltage status
Use the Right Arrow button on the top-right corner of the screen to view the following information:
-
Current and voltage per phase (I-V)
-
Energy (E)
-
Power per phase (P)
-
Total power and energy (P-E)

DANGER
WARNING