990-5936G-001

Clearance

NOTE: Clearance dimensions are published for airflow and service access only. Consult with the local safety codes and standards for additional requirements in your local area.
NOTE: 914 mm (36 in) left side clearance is only required for non-routine transformer service such as transformer tap changes and main current transformer replacement. For routine operation and maintenance of the PDU, there is no side clearance required.

Front View of the PDU – Standard Unit

Front View of the PDU – With the Infrared Window

*For PDUs installed with the optional infrared window, a right side clearance of 635 mm (25 in) is required.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.