990-5936G-001

Configure the System

  1. From the home screen on the display select Configuration > System.
  2. Set System Output Voltage to 400 V or 208 V or 415 V or 216 V as per your system.
  3. Set Input Protection to Switch or Breaker as per your system.
  4. Set Output Protection to Not Installed or Breaker as per your system.
  5. Set Input Meter to None, EM3550, or PM5564 as per your system.
  6. Set Output Meter to EM3550, PM5564, or PM8244 as per your system.
  7. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.