990-5936G-001

Position the PDU

  1. Move the PDU to the final installation location with a forklift. Lift the PDU front to back or back to front through the openings in the lower part of the PDU.
    WARNING
    Tipping hazard
    The PDU is very heavy and contains a very heavy transformer. When lifting the PDU with a forklift, keep the PDU as level as possible. Do not tilt the PDU while lifting it. Only use a forklift to lift the PDU, never use a pallet truck.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.