990-5936G-001

Edit or Delete a Branch Circuit Breaker

  1. From the home screen on the display select Configuration > Branch > Edit Breaker.
  2. Select the Position for the branch circuit breaker and select Modify Breaker to edit the branch circuit breaker parameters or Delete Breaker to delete the branch circuit breaker from the configuration.
    NOTE: If an alarm exists for a given branch circuit breaker, you must reboot the display after deleting a circuit breaker to clear the alarm(s).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.