990-5936G-001

Storage

If the equipment is to be stored prior to installation, it should be stored in a cool, dry, well-ventilated location that is protected against rain, splashing water, chemical agents, etc. The equipment should be covered with a tarpaulin or plastic wrapper to protect it against dust, dirt, paint, or other foreign materials.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.