990-5936G-001

Configure the Output Parameters

  1. From the home screen on the display select Configuration > Output.
  2. Enable the Breaker Open Alarm, if needed.
  3. Set the Voltage Thresholds for: Maximum, High, Low, and Minimum by tapping Enable and setting the percentage.
  4. Tap the > symbol to go to the next page.
  5. Set the Current Thresholds for: Maximum, High, Low, and Minimum by tapping Enable and setting the percentage.
  6. Set the Apparent Power Thresholds for: Maximum and Minimum by tapping Enable and setting the percentage.
  7. Tap the > symbol to go to the next page.
  8. Set the Misc Thresholds for: Over Active Power, PF Deviation, Phase Loss, and Frequency Deviation by tapping Enable and setting the percentage or choosing from the drop-down list.
  9. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.