990-5936G-001

Configure a Branch Circuit Breaker

  1. From the home screen on the display select Configuration > Branch > Add Breaker.
  2. Configure the branch circuit breaker parameters:
    1. Set the Position to: TOP/BOTTOM and type the position number.
      The positions are assigned taking the center as a reference:

      Branch Circuit Breaker Positions

      TOP 7
      TOP X
      TOP 2
      TOP 1
      Center
      BOTTOM 1
      BOTTOM 2
      BOTTOM X
      BOTTOM 7
    2. Set the Associated Channels for L1. L2 and L3 will be populated automatically.
    3. Set the Breaker Rating current (1–600).
    4. Set the CT Size (0–2000).
    5. Set the I2C Position (1–14).
    6. Tap the > symbol to go to the next page to provide optional settings, or tap OK to use default settings for the next two pages.
    7. Set the Load Identifier for the circuit breaker.
    8. Enable Alarm Generation, if needed.
    9. Enable Breaker Open Alarm, if needed.
    10. Set the Apparent Power Thresholds for: Maximum and Minimum by tapping Enable and setting the percentage.
    11. Tap the > symbol to go to the next page.
    12. Set the Current Thresholds for: Maximum, High, Low, and Minimum by tapping Enable and setting the percentage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.