990-5936G-001

Install the Anchoring and Position the PDU

Overview of Anchoring Holes

  1. Drill holes for anchoring in the floor according to the overview.
  2. Mount the three rear anchors to the floor with M12 bolts (not provided).

    Rear View of the PDU

  3. Move the PDU to the final installation location with a forklift. Lift the PDU front to back or back to front through the openings in the lower part of the PDU.
    WARNING
    Tipping hazard
    The PDU is very heavy and contains a very heavy transformer. When lifting the PDU with a forklift, keep the PDU as level as possible. Do not tilt the PDU while lifting it. Only use a forklift to lift the PDU, never use a pallet truck.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  4. Install the rear anchoring brackets on the PDU.
  5. Push the PDU into position with the forklift so the rear anchoring brackets connect to the rear anchors.
  6. Install the front anchoring brackets on the PDU and mount to the floor with M10 expansion bolts (not supplied).

    Front View of the PDU

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.