990-5936G-001

Prepare the PDU for Cables in Top Entry System

DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or conduits with the gland plate installed and do not drill or punch holes in close proximity to the PDU.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the right side panels and left side panels from the PDU for better access, if possible.
  2. Remove the indicated front plates.
  3. Remove the gland plates from the top of the PDU.

    Front View of the PDU

  4. Drill/punch holes for power cables/conduits in the gland plates. Conduits are not provided.
  5. Reinstall the gland plates in the top of the PDU.
  6. Lockout/Tagout the main input circuit breaker MIB/main input switch MIS in the OFF (open) position.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.