990-5936G-001

Connect the Input Power Cables

  1. Route the equipment grounding conductor/PE cables through the top or bottom left side of the PDU and connect to the PE busbar.
  2. Route the input cables through the top or bottom left side of the PDU and connect to the main input circuit breaker MIB/main input switch MIS.

    Front View of the PDU

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.