990-5936G-001

User Interface

Front View of the PDU (Display Model 1)

Front View of the PDU (Display Model 1)

  1. PDU display*

  2. EPO (emergency power off) button (option)

  3. Power meter (option)

  4. Power meter (option)

  5. Status LEDs

  6. Display reset button

  7. Network connection LED:

    • Solid green: The system has valid TCP/IP settings.

      See Configure the Network.

    • Flashing green: The system does not have valid TCP/IP settings.

    • Solid orange: The display is inoperable. Contact Schneider Electric.

    • Flashing orange: The system is making BOOTP requests.

      See Configure the Network.

    • Alternately flashing green and orange: If the LED is alternately flashing slowly, the system is making DHCP requests.

      See Configure the Network.

      If the LED is alternately flashing rapidly, the system is starting up.

    • Off: The display is not receiving input power or the display is inoperable.

  8. LED for indication of network connection type:

    • Solid green: The system is connected to a network operating at 10 Megabits per second (Mbps).

    • Flashing green: The system is receiving or transmitting data packets at 10 Megabits per second (Mbps).

    • Solid orange: The system is connected to a network operating at 100 Megabits per second (Mbps).

    • Flashing orange: The system is receiving or transmitting data packets at 100 Megabits per second (Mbps).

    • Off: One or more of the following exists: The display is not receiving input power, the cable that connects the system to the network is disconnected, the device that connects the system to the network is turned off, or the display is inoperable. Check the connections and if the LED remains off, contact Schneider Electric.

  9. Slots reserved for service.

  10. USB port.

Overview of Status LEDs

Power LED: The PDU is powered when the LED is illuminated. PDU firmware is being updated when the LED is flashing.
Check log LED: When the LED is illuminated, a new PDU entry has been made in the event log.
Alarm LED: When the LED is illuminated, there is an alarm condition in the PDU system.

Power Meter Operation

Follow the documentation delivered with the specific power meter for operation, maintenance, and troubleshooting.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.