990-5936G-001

View the System Status Information

  1. From the home screen on the display select Status and select the area that you want to see the status for.
    NOTE: IF the PDU does not have an input meter installed, the input status screen will only show Breaker State:Open/Closed.

    Input

    Current

    The present input current from the AC utility power source per phase in amperes (A).

    Energy Usage

    The accumulated input energy (kWh)

    Frequency

    The present input frequency in hertz (Hz).

    Breaker Status

    The present circuit breaker status, either Open or Closed.

    Voltage (phase-to-phase)

    The present phase-to-phase input voltage.

    NOTE: The different meters support different output parameters; The PDU display may not show all of the output parameters listed.

    Output

    Voltage (phase-to-neutral)*

    The phase-to-neutral output voltage in volts (V).

    Current

    The present output current for each phase in amperes (A).

    Active Power

    The present active power (or real power) output for each phase in kilowatts (kW). Active power is the portion of power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.

    Reactive Power

    The present reactive power for each phase in kVAR. Reactive power represents energy alternately stored and released by inductive and capacitive loads in the system.

    Apparent Power

    The present apparent power output for each phase in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Power Factor

    The present output power factor for each phase. Power factor is the ratio of active power to apparent power.

    Displacement PF

    The present output displacement power factor for each phase. Displacement power factor is the ratio of active power to apparent power considering the fundamental frequency (60 Hz) only, and neglecting the harmonics.

    Frequency

    The present output frequency in hertz (Hz).

    Breaker Status

    The present circuit breaker status, either Open or Closed.

    Voltage (phase-to-phase)

    The phase-to-phase output voltage in volts (V).

    Active

    Active energy - The total active energy consumption since the unit was energized, in Watts-hour (Wh).

    Reactive

    Reactive energy - The total reactive energy consumption since the unit was energized, in VARh.

    Apparent

    Apparent energy - The total apparent energy consumption since the unit was energized, in Volt-Ampere-hour (VAh)

    Total Active Power

    The present total active output power (for all three phases) in kilowatts (kW).

    Total Apparent Power

    The present apparent power output for each phase in thousands of Volt-Amps (kVA). Apparent power is the product of RMS (root mean square) volts and RMS amperes.

    Total Reactive Power

    The present total reactive power in kVAR.

    Total Power Factor

    The present total power factor.

    Total Displacement PF

    The present total displacement power factor.

    Energy Reset Date

    The date and time since the unit was first energized and the accumulated energy has been measured.

    System

    Output Voltage

    The phase-to-phase output voltage in volts (V).

    Output Current

    The present output current for each phase in amperes (A).

    Output Frequency

    The present output frequency in hertz (Hz).

    Output Voltage (L-N)

    The present phase-to-neutral output voltage in volts (V).

    System Time

    The time of the PDU system.

    Power Factor

    The present output power factor.

    Breaker Status

    The present output circuit breaker status, either Open or Closed.

    Total Output Power

    The apparent and active power (or real power) output for each phase.

    Output Power

    The phase-to-phase apparent and active power (or real power) output for each phase.

    Active Alarms

    Active Alarms

    For more information on active alarms, go to View the Active Alarms.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.