990-5936G-001

Final Installation

  1. Reinstall all removed plates in the PDU.
  2. Reinstall the side panels on the PDU.
  3. Install the kick plates on all sides of the PDU.

    Front View of the PDU

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.