990-5936G-001

View the Log

  1. From the home screen on the display select Logs.
  2. You can browse through the list of the events using the arrows.
  3. You can now perform the following operations in the event log:
    1. Tap the filter button to filter the events. Different filter settings are available.
    2. Tap the recycle bin button to clear the event log and select Yes to confirm.
  4. Tap the home button to exit the log.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.