990-5936G-001

Find the Serial Numbers

NOTE: If the display is not available, the serial number can also be found on a label in the cabinet.
  1. From the home screen on the display tap About.
  2. Tap on PDU and note down the serial number and have it ready for customer support.
  3. Tap on the About in the top of the screen to go back.
  4. Tap on Display and note down the serial number and have it ready for customer support.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.