990-91405J-001

Efficiency

Efficiency in Battery Mode

UPS rating 10 kVA 20 kVA 30 kVA 40 kVA 60 kVA 80 kVA 100 kVA 120 kVA 160 kVA 200 kVA
25% load

77.58

90.49

89.13

88.73

89.63

91.16

89.86

90.38

91.47

91.51

50% load

85.91

92.64

91.91

91.55

92.39

93.42

92.89

93.07

93.48

93.53

75% load

88.74

92.33

92.32

92.23

92.87

93.67

93.34

93.53

93.65

93.68

100% load

90.07

92.24

92.11

92.28

92.76

93.47

93.29

93.48

93.58

93.25

Efficiency in ECO Mode

UPS rating 10 kVA 20 kVA 30 kVA 40 kVA 60 kVA 80 kVA 100 kVA 120 kVA 160 kVA 200 kVA
25% load

80.4

87.53

88.96

91.48

91.79

92.02

89.25

90.09

91.13

91.39

50% load

88.73

92.81

94.08

94.95

95.05

95.51

94.05

94.56

95.07

96.67

75% load

91.21

95.43

95.75

96.53

96.58

96.94

95.74

96.15

96.55

97.05

100% load

93.67

96.21

96.61

97.27

97.27

97.51

96.58

96.88

97.11

97.69

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.