990-91405J-001

Options

Configuration Options

  • Single or dual mains

  • Up to four UPSs in parallel – 3+1 for redundancy and 4 for capacity

  • ECO mode

Hardware Options

NOTE: All hardware options listed here may not be available in all regions.
  • Backfeed kit for Galaxy PW 2nd Gen 10 to 30 kVA 3:1 (EPWOPT015)

  • Backfeed kit for Galaxy PW 2nd Gen 10 to 120 kVA 3:1 (EPWOPT016)

  • Galaxy PW 2nd Gen 10-60 kVA, IP42 kits for 800 mm width cabinets (EPWOPT017)

  • Galaxy PW 2nd Gen 60-80 kVA, IP42 kits for 800 mm width cabinets (EPWOPT018)

  • Galaxy PW 2nd Gen, IP42 kits for 1200 mm width cabinets (EPWOPT019)

  • Galaxy PW 2nd Gen, IP42 kits for 1600 mm width cabinets (EPWOPT020)

  • Network management card (AP9547)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.