990-91405J-001

EPO

Only use the EPO button in case of emergency.

When the EPO is activated, the UPS will:

  • turn off the rectifier, inverter, charger, and static bypass and stop supplying the load immediately (default).

NOTE: When the EPO is activated, the load will drop for both single and parallel systems.
DANGER
hazard of electric shock, explosion, or arc flash
The UPS control circuit will remain active after the EPO has been pushed if mains is available.
Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.