990-91405J-001

Location of Disconnect Devices

Locations of Disconnect Devices on the 3:1 UPSs

10-40 kVA 3:1 220 VDC UPS

50-80 kVA 3:1 220 VDC UPS

100-120 kVA 3:1 220 VDC UPS

10-40 kVA 3:1 384 VDC UPS

60-80 kVA 3:1 384 VDC UPS

Locations of Disconnect Devices on the 3:3 UPSs

10-80 kVA 3:3 384 VDC UPS

100-120 kVA 3:3 384 VDC UPS

160-200 kVA 3:3 384 VDC UPS

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.