990-91405J-001

Drawings

NOTE: A comprehensive set of drawings is available on www.se.com.
NOTE: These drawings are for reference ONLY – subject to change without notice.

Galaxy PW 2nd Gen 3:1 Single System

3:1 220 VDC UPS

3:1 384 VDC UPS

Galaxy PW 2nd Gen 3:1 1+1 Redundant Parallel System

3:1 220 VDC UPS

3:1 384 VDC UPS

Galaxy PW 2nd Gen 3:3 Single System

3:3 384 VDC UPS

Galaxy PW 2nd Gen 3:3 1+1 Redundant Parallel System

3:3 384 VDC UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.