990-91262E-001

Prepare for Signal Cables

  1. Remove the top gland plates and the top brush plates from the UPS. These are for signal cable routing.
  2. Perform one of the following:
    • For installation without conduits: Reinstall the brush plates.
    • For installation with conduits: Drill a hole in the gland plates for conduits, install conduits, and reinstall the gland plates.
  3. Remove the indicated covers.
  4. Route the non-Class 2/non-SELV signal cables through the right brush/gland plate.
  5. Route the Class 2/SELV signal cables through the left and middle brush/gland plate.

    UPS without Conduits

    UPS with Conduits

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?