990-91318H-001

Batteries

End of Discharge Voltage

The voltage is 1.6 to 1.75 per cell depending on discharge ratio.

Battery Voltage Window

  Boost 2.38 Vpc Nominal 2.0 Vpc Minimum 1.6 Vpc
Battery voltage (V) 571.2 480 384

Battery Runtimes in Minutes

480 V UPS

UPS rating 20 kW
Number of modular battery strings
1 NA
2 8.4

208 V UPS

UPS rating 10 kW
Number of modular battery strings
1 8.3
2 22
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.