990-91318H-001

Efficiency

20 kW Normal operation Battery operation
25% load 90.1% 92.4%
50% load 92.1% 94.9%
75% load 93.2% 95.8%
100% load 93.8% 96.2%
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.