990-91318H-001

Derating Due to Load Power Factor

0.7 leading to 0.7 lagging without derating.

UPS rating UPS output
Lagging Leading
PF=1 PF=0.7 PF=0.8 PF=0.9 PF=0.9 PF=0.8 PF=0.7
20 kVA/kW 20 kVA / 14 kW 20 kVA / 16 kW 20 kVA / 18 kW 20 kVA / 18 kW 20 kVA / 16 kW 20 kVA / 14 kW
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.