990-91318H-001

Compliance

Safety UL 1778 5th edition
EMC/EMI/RFI FCC Part 15 Subpart B, Class A
Seismic ICC-ES AC 156 (2015): OHSPD Pre-approved; Sds=1.54 g for z/h=1 and Sds=1.63 g for z/h=0; Ip= 1.5
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.