990-91318H-001

Drawings

NOTE: A comprehensive set of drawings is available on www.se.com.
NOTE: These drawings are for reference ONLY – subject to change without notice.

20 kW 480 V and 10 kW 208 V

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.