EIO0000003527.05

Status LED

After power is turned on, normal status indicated by the LED is: red light > blinking orange > green light.

Color Indicator HMI operation
Green ON In operation
Flashing once every 5 seconds Backlight OFF (Standby Mode)
Orange Blinking Software starting up
Red ON Power is ON.
- OFF Power is OFF.

For other LED indications, refer to the manual of your screen editing software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?