DOCA0147EN-17

User Management Reconfiguration after Firmware Update

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
LOss of data
  • Ensure that you take backup of the data log files before updating the firmware. The data log entries of the IFE or EIFE interface may be lost when the firmware is updated.
  • Ensure that you take backup of data present in User Accounts and Email Events sections of IFE or EIFE webpages.
  • Ensure that after firmware upgrade, you restore the User Accounts and Email Events configuration on IFE or EIFE webpages.
Failure to follow these instructions can result in permanent loss of data.

To take advantage of new security features, the reconfiguration of the
IFE or EIFE webpage users is required when an IFE or EIFE interface firmware is updated from a version 003.010.005 or earlier to 004.001.000 or later.

The management of the users of the IFE or EIFE webpages for firmware version 004.001.000 or later is based on Role Base Access Control (RBAC). It is not compatible with the user management of the IFE or EIFE webpages for firmware version 003.010.005 or earlier.

After the firmware update of an IFE or EIFE interface from a version 003.010.005 or earlier to 004.001.000 or later:

  • The Guest account is removed.

  • The Administrator account is removed and replaced by a SecurityAdmin user:

    • With the default password: AAAAAAAA.

    • With the email address of the Administrator account

      .
  • The first 11 configurable user accounts are maintained:

    • With the same user names. If a user name was shorter than four characters, then 0 are added to complete it to four characters.

    • With the same email addresses.

    • With the default password: Admin@123

    • With Viewer role.

  • The last three configurable accounts are removed.

  • The export of logging data by email is disabled.

  • The notification of email events is reset to default values.

  • The email addresses for notifications are removed.

Once the IFE or EIFE interface firmware is updated from a version 003.010.005 or earlier to 004.001.000 or later, the Security Administrator must edit and review the user accounts configuration on the USER MANAGEMENT webpage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?