DOCA0147EN-17

Firmware Version 005.001.000

New Features

The following features are added:

  • Read Device Registers feature for IFE or EIFE interface to read Modbus registers from the selected device.

  • Integration of BSCM Modbus SL/ULP module which is compatible with IFE interface only.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?