DOCA0147EN-17

Firmware Version 004.007.000

Security Updates

Enhanced cybersecurity features.

New Features

The following features are added:

  • Syslog logging service feature.

  • Machine-to-Machine (M2M) communication for Modbus communication.

  • Role Base Access Control (RBAC) for MasterPacT MTZ with MicroLogic X control unit.

  • Reset security administrator password.

Known Issues

The Diagnostics page for RSTP goes blank when the RSTP service is disabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?