DOCA0147EN-17

Firmware Version 003.012.002

New Features

Added MicroLogic Xi control units. A MicroLogic Xi is a control unit without Bluetooth Low Energy (BLE) communication.

Bugs Fixed

Time synchronization of IFM interface with IFE or EIFE interface did not happen when the IFE or EIFE interface was in Daylight Saving mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?