DOCA0147EN-17

Firmware Version 004.004.001

Security Updates

The following security updates are done:

  • Enhanced cybersecurity features.

  • Included the patch for IPv6 vulnerabilities.

New Features

The new range of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers are introduced with the evolution of existing ComPact NSX and PowerPact H-, J-, and L-frame range of circuit breakers.

Bugs Fixed

The measurement values were inconsistent with the real time values after the IMU system recovered from critical discrepancy.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?