DOCA0147EN-17

Firmware Version 004.003.000

New Features

The new range of ComPacT NSX and PowerPacT H-, J-, and L-frame circuit breakers are introduced with the evolution of existing ComPact NSX and PowerPact H-, J-, and L-frame range of circuit breakers.

Bugs Fixed

The following bugs are fixed:

  • Language and phone number was not updated while creating a user account.

  • Location field was removed from the user account pages.

  • After the firmware was upgraded from 003.xxx.xxx to 004.002.000, the HTTPS protocol was not enabled by default.

  • After the firmware was upgraded from 003.xxx.xxx to 004.002.000, the FTP protocol was disabled.

  • The register 12395 for freshness timeout setting was not always accessible without the installation of the Modbus Legacy Dataset Digital Module.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?