Firmware Version 003.009.010
New Features
The following maintenance features are added and are available with a MicroLogic X control unit with firmware version 003.011.000 or later:
-
New events for contact wear ratio.
-
New events for type of preventive maintenance to be performed.
Access has been added through Modbus registers to the following data for MasterPacT MTZ circuit breakers:
-
Average peak current demand.
-
Minimum and maximum values of real-time measurements.
-
Energy per phase values.
-
Main settings of the active setting group of current protection functions.
Bugs Fixed
The following bugs are fixed:
-
IFE or EIFE interface lost its clock master status when SNTP server did not answer.
-
IFE or EIFE interface restarted when discovery packet from Satchwell Sigma BMS platform was received.