DOCA0147EN-17

Firmware Version 004.009.000

Security Updates

Restored compatibility with EcoStruxure Cybersecurity Admin Expert software version 2.4.3 and later.

New Features

Role Base Access Control (RBAC) has been added for ComPacT NSX with MicroLogic 5, 6, and 7 trip units.

Bugs Fixed

The IFE or EIFE webpage did not load on certain versions of Google Chrome.

NOTE: The above bug was observed in Google Chrome version 107.0.5304.63 (official build) (64 bit).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?