DOCA0147EN-17

Firmware Version 004.010.000

Security Updates

Enhanced cybersecurity features.

New Features

The following features are added:

  • Device Specific Settings (DSS) feature that enables the IFE or EIFE interface configurations to be tailored for each individual device.

  • Signature verification feature to validate the security configuration files received from EcoStruxure Cybersecurity Admin Expert software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?