DOCA0147EN-17

Firmware Version 003.011.003

New Features

The events are added for internal Current Power Supply (CPS) sensors, available with the MicroLogic X control unit for firmware version 004.105.000 or later.

Bugs Fixed

Treck TCP/IP Vulnerabilities (Ripple20)

For more information, refer to SEVD-2020-175-01 Schneider Electric Security Notification.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?