Firmware Version 003.006.011
New Features
The following features are added for IFE or EIFE interface:
-
Access has been added through Modbus registers to the trip cause data for MasterPacT MTZ circuit breakers.
-
Support of alpha-numeric passwords for IFE webpages.
The following features are added for IFE interface:
-
Support for the internal battery that maintains the date and time settings of the real-time clock (RTC) during a power loss (reference LV434001).
-
Compatibility with ULP cables up to 20 m (65 ft) in length.
-
Alarm support for the MicroLogic P and H advanced protection settings, allowing an alarm email to be sent.
-
Discovery from IFE webpages of devices equipped with non-communicating trip units, through BCM or BSCM module (e.g. NSX non-communicating MicroLogic with BSCM module), for device status display only.
-
Compatibility with new MicroLogic 7 trip units for ComPacT NSX circuit breakers.
Bugs Fixed
The following bug is fixed for IFE or EIFE interface:
-
FTP server could not be enabled in Italian language.
The following bug is fixed for IFE interface:
-
BCM firmware update was not performed when IFE interface closed connection in DHCP mode.