DOCA0147EN-17

EIFE Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker

The EIFE interface with part number LV851001 enables one MasterPacT MTZ drawout circuit breaker to be connected to an Ethernet network.

It provides:

  • Digital access to all the data that is delivered by the MicroLogic Active or MicroLogic X control unit of the MasterPacT MTZ circuit breaker.

  • Information about the IMU system.

It also monitors the three positions of the circuit breaker in the cradle:

  • Cradle connected

  • Cradle disconnected

  • Cradle test position

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?