DOCA0147EN-17

Firmware Version 003.010.005

New Features

Access has been added through Modbus registers to the following data for MasterPacT MTZ circuit breakers:

  • IDMTL protection trip

  • Over/Under frequency trip

  • Directional overcurrent trip

  • Discrepancy between display and MicroLogic control unit

Bug Fixed

When IP Filtering was enabled as Read only, the Modbus function Scattered read was blocked.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?