DOCA0147EN-17

Firmware Version 003.007.024

New Features

The following features are added for IFE or EIFE interface and are available with a MicroLogic X control unit with firmware version 002.000.003 or later:

  • Monitoring of current and power demand values.

  • Reset of peak demand values.

  • New events for notification by email:

    • Presence of 24 Vdc power supply.

    • Ground-fault alarm or Earth-leakage alarm (available when Ground-fault Digital Module is installed on MicroLogic X control unit).

  • Update of standard dataset with current and power demand values.

  • Availability of legacy dataset when Modbus Legacy Dataset Digital Module is installed on the MicroLogic X control unit.

  • Availability of individual harmonics and currents up to rank 40 when Individual Harmonics Analysis Digital Module is installed on the MicroLogic X control unit.

  • Introduction of new mechanism for activating Digital Modules across Enerlin’X devices.

  • Modification to management of multiple requests through command interface: reception of new command aborts previous command still in progress.

The following features are added for IFE interface:

  • ComPacT NSX circuit breaker with MicroLogic 7 trip unit as discoverable device that can be connected to ULP port of IFE interface.

Bugs Fixed

The following bug is fixed for IFE interface:

  • LV434001: ULP LED was blinking green instead of yellow when IFE interface was in Boot mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?